Post Go back to editing

ADuM120N: different VDD apply

Thread Summary

The user inquires about using ADuM120N Digital Isolators to send PWM signals from a 3.3V microcontroller to motor drivers with a 5V supply. The final answer confirms that VDD1 and VDD2 can be different, making the configuration in the provided diagram acceptable.
AI Generated Content
Category: Datasheet/Specs
Product Number: ADuM120N

Hi, I'm finding 2 (or 6) chanel Digital Isolators to send PWM from uC to MotDrivers.

I'm looking ADuM120N.

Can ADuM120N supports different VDD (VDD1 = 3V3, VDD2 = 5V)?

DIN_1, 2 is from 3V3 uC, So, VDD1 can't be 5V (not reach 0.7VDD)

While At Isolated VDD2 side has only 5V supply.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.