Post Go back to editing

Is the internal reference voltage of the ADuM6212 1.225V?

Category: Datasheet/Specs
Product Number: ADuM6212

Hello.

I have questions about ADuM6212.

The internal reference of the ADuM6212 is listed as 1.25V, but the VISO formula is 1.225V.

Is the internal reference voltage of the ADuM6212 1.225V?
Also, does the internal reference voltage vary from 1.225V depending on temperature and other factors?

Best regards,

Parents Reply
  • Hi miky,

    The reference voltage is meant to match up to the 1.25V. You can focus on the Viso range to meet that refence voltage value. The margin for Viso is 20% to cover any temperature variations. Based off this, I advise to have your refence voltage within this same range to avoid any potential issues: between 1V and 1.5V.

    Regards,

    amitmadan

Children
No Data