Hi,
We have a design implementing the LTC4306 on a backplane to provide I2C to 4 downstream modules. In some scenarios, 1 or more of these modules may be present.
We would like to use the 'Downstream Bus Connection Fault" to detect if a module is missing, which requires less than 1V on the downstream SDA/SCL pins.
Is the suggested implementation for this to have the downstream I2C pullup resistors on the module, so that the downstream bus pins of the LTC4306 are floating when no module is connected?
Or do we need to include a weak pulldown on the backplane to ensure the downstream bus pins are below the 1V threshold?
Thanks in advance for your support.
Cooper