Post Go back to editing

I2C bus pull up for AD5245

Thread Summary

The user experienced unreliable communication with the AD5245, potentially due to pull-up resistor issues. The final solution involved changing the pull-up resistor from 10kΩ to 2.2kΩ, which improved the communication. The user also noted that the issue was resolved when connecting an oscilloscope, suggesting a possible edge detection problem.
AI Generated Content
Category: Hardware
Product Number: AD5245BRJZ5

The communication with the AD5245 is sometimes not successful. It may be a pull-up problem. Can you tell me which values are good for the pull-up for this device. I am using 10k resistors for the pull up.

Parents Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.