Hello
I'm considering the ADN4697E.
I have a question about the circuit behavior when the receiver switches from OFF to ON.
①Please tell me the time required for the threshold of the internal comparator that detects A-B to stabilize after RE turns ON (High → Low).
②When DE is switched from High to Low with RE set to Low, is there any waiting time required from RE(Low) to DE(Low)?
I would like to use ADN4697E to achieve movement similar to ADN4696E.
When the ADN4697E is not communicating with the master, I would like to keep the receiver on and watch the communication so that I can get the signal of another slave unit.
However, when the receiver is turned OFF, not only the receiver but the entire circuit is turned OFF, and when it is turned ON, the circuit starts from starting up.
Therefore, it will take some time for the internal comparator threshold to stabilize, so I will mask the judgment using the MCU for a while when RE is changed from High to Low.