Post Go back to editing

ADUM141ES Output Impedance

Thread Summary

The user is experiencing non-monotonic signals at the receiving circuit when using an ADuM141ES at 5V. The output stage is push-pull CMOS and not designed to drive a 50Ω load, potentially violating the ±10mA output current limit. The output impedance is in the 60-80Ω range, and the issue does not occur at 3.3V with a 33.2Ω source termination. The user is advised to contact technical support for further assistance.
AI Generated Content
Category: Hardware
Product Number: ADUM141ES

Is there any information available about the output impedance of the VOA, VOB, VOC and VOD outputs? I would like to best match the output impedance to the trace transmission line impedance. I tried to ask this same question on an older thread over a month ago, but got no replies.

Ideally, I'd like to have an IBIS model, but the output impedance will do for now.

 

For reference, we are seeing what appears to be a non-monotonic signal at the receiving circuit (high impedance digital input) of a signal that originates from an ADuM141ES operating at 5V. We have a source series termination resistor and the trace between the ADuM141ES output and the receiving circuit is designed with a 50Ω impedance. We've varied the source termination resistor and have not been able to remove the non-monotonicity. We've also wired in a parallel load termination resistance of 680Ω and that also has not helped.

Parents
  • Hi, 

    The ADuM141ES is derived from the ADuM141E industrial grade. There are probably some differences between package parasitics but might be good enough for your purpose.  

    The output stage is push-pull CMOS. Its not meant to drive a 50Ω load and the design is likely violating the abs max average current of ±10mA on the output pin. 

    Try reaching out to technical support if you need additional support on the ADuM141ES. https://www.analog.com/en/support/technical-support.html# 

    Regards,

    Jason

  • Thanks for the fast reply Jason! I'm a little confused about your comment stating that it's not meant to drive a 50Ω load and violating the max pin current. This is a high-speed device, so what characteristic impedance is it intended to drive into?

    Also, we only see this when operating at 5V on the VDD2 side. The other side is at 3.3V (VDD1) with a 33.2Ω source term. and we don't see any non-monotonicities.

    I will also reach out to tech support separately.

Reply
  • Thanks for the fast reply Jason! I'm a little confused about your comment stating that it's not meant to drive a 50Ω load and violating the max pin current. This is a high-speed device, so what characteristic impedance is it intended to drive into?

    Also, we only see this when operating at 5V on the VDD2 side. The other side is at 3.3V (VDD1) with a 33.2Ω source term. and we don't see any non-monotonicities.

    I will also reach out to tech support separately.

Children
  • Hi, 

    Typically a standard data isolator is driving a high impedance CMOS input. The output impedance is in 60-80Ω range but loading the output heavily will probably pull the output high level below what's needed for 3.3V or 5V CMOS logic. The LEO parts are there own expertise which is why I recommend contacting technical support, but the abs max rating I'm referring to is "Output current per pin" in section 4.1   

    Regards,

    Jason

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.