Post Go back to editing

Alternative Spice model for MAX22700EASA+

Thread Summary

The user is looking for a Spice model for the MAX22700EASA+ gate driver. Analog Devices suggests using the MAX22701D model from LTSpice, which is available after updating the components library. The MAX22701D has a differential input and Miller clamp feature, while the MAX22700E has an ENABLE pin and a separate GNDB pin. The MAX22701D model is encrypted and cannot be exported to Ansys Electronics for signal/power integrity analyses.
AI Generated Content
Category: Hardware
Product Number: MAX22700EASA+, MAX22700E

Hi, 

I have used gate driver MAX22700EASA+ in my design, and need its Spice model for verification purposes. Analog device does not have any Spice models of the MAX22700E available, BUT is there any other similar driver (same family) that I can use its Spice model as an alternative to MAX22700E ?

BR

Parents
  • Hi,

    thanks for your question. Recently we have released the model for the MAX22701D, which belongs to the same family of the MAX22700E. The MAX22701D model could be found in LTSpice after updating the components library (Tools -> Update components).

    The main differences between the two components are:

    1) the MAX2270xD has a differential input while the MAX2270xE has a ENABLE pin. This affects the way you command the gate driver but not the actual gate driving performances

    2) the MAX22701 has a Miller clamp feature while the MAX22700 has a dedicated gate driver common pin (GNDB) separated from the negative power supply of the side-B (VSSB).

    If you don't have special requirements, I suggest you to try the available model.

    Which is the application you want to address?

    Alessandro

Reply
  • Hi,

    thanks for your question. Recently we have released the model for the MAX22701D, which belongs to the same family of the MAX22700E. The MAX22701D model could be found in LTSpice after updating the components library (Tools -> Update components).

    The main differences between the two components are:

    1) the MAX2270xD has a differential input while the MAX2270xE has a ENABLE pin. This affects the way you command the gate driver but not the actual gate driving performances

    2) the MAX22701 has a Miller clamp feature while the MAX22700 has a dedicated gate driver common pin (GNDB) separated from the negative power supply of the side-B (VSSB).

    If you don't have special requirements, I suggest you to try the available model.

    Which is the application you want to address?

    Alessandro

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.