i2c issue in communication using 
ADuM1440
Recommended for New Designs
The ADuM1440/ADuM1441/ADuM1442/ADuM1445/ADuM1446/ADuM1447 are micropower, 4-channel digital isolators based on the Analog Devices, Inc., iCoupler® technology...
Datasheet
ADuM1440 on Analog.com
ADUM1252
Recommended for New Designs
The ADuM1252 offers two bidirectional, open-drain
channels for applications, such as I2C, that require data
to be transmitted in both directions on the...
Datasheet
ADUM1252 on Analog.com
i2c issue in communication using 
Hi,
I2C always requires at least a bidirectional SDA line so a peripheral can send back an ACK bit and data to the MCU. The SCL line may or may not need to be bidirectional; it depends on what peripherals are being used and if they need to do something like clock stretching.
The ADuM1440 has 4 unidirectional channels, so it will not work for I2C bus isolation. Communication in the direction of the wireless base board is not possible in the schematics above, and the push/pull outputs of the ADuM1440 may even be causing communication issues on the MCU side.
There is an ultra-low power I2C isolator in the ADI portfolio. I recommend considering the ADuM1252.
Regards,
Jason
Hi,
I2C always requires at least a bidirectional SDA line so a peripheral can send back an ACK bit and data to the MCU. The SCL line may or may not need to be bidirectional; it depends on what peripherals are being used and if they need to do something like clock stretching.
The ADuM1440 has 4 unidirectional channels, so it will not work for I2C bus isolation. Communication in the direction of the wireless base board is not possible in the schematics above, and the push/pull outputs of the ADuM1440 may even be causing communication issues on the MCU side.
There is an ultra-low power I2C isolator in the ADI portfolio. I recommend considering the ADuM1252.
Regards,
Jason