Hello ADI support team,
According to the datasheet of the MAX13451E it should indicate a short circuit condition (on the RS485 bus) with a HIGH FAULT output, but we can't get this feature working.
We see the following with VCC = 5V, VL = 1V8, SRL = INV = TERM100 = nTERM = 0V, DE = nRE = DI = 1V8, 100 kOhm pull-down resistor on the FAULT pin:
- With no errors on the bus signals we can measure ~60 mV at the FAULT pin
- With the A+B signals shorted together we can measure ~200 mV at the FAULT pin
- With the A+B signals connected to GND we can measure ~200 mV at the FAULT pin
- With either of the A or the B signals connected to 6V (over-voltage condition) we can see a valid HIGH state at the FAULT pin
What can be the issue?
Thanks for any help.