Hello
I am looking for an alternative to this reference but its quite difficulte to find an exacte replacement, do you have any suggestion ?
1B22
Last Time Buy
The 1B22 is an isolated voltage-to-current converter that incorporates transformer isolation to achieve high performance and automated surface mount manufacturing...
Datasheet
1B22 on Analog.com
1B21
Obsolete
The 1B21 is an isolated voltage-to-current converter that
incorporates a unique circuit design utilizing transformer-based
isolation and automated surface...
Datasheet
1B21 on Analog.com
AD693
Production
The AD693 is a monolithic signal conditioning circuit which accepts low-level inputs from a variety of transducers to control a standard 4-20 mA, two-wire...
Datasheet
AD693 on Analog.com
Hello
I am looking for an alternative to this reference but its quite difficulte to find an exacte replacement, do you have any suggestion ?
Hi TCW,
Unfortunately, we do not have a drop-in replacement for the 1B22 available at this time. Below are some potential alternatives:
There is also a library of Reference Designs and there may be something for isolated 0 V to +5 V or 0 V to +10 V inputs conversion to 4 to 20 mA outputs.
Regards,
Jason
would you have any suggestion also for the 1B21 ?
Hi,
Same as above.
I guess there will need to be a redesign of some sorts here. CN0382 or CN0376 aren't exactly what you need, but they are the direction I'd imagine to go starting fresh. An ADC (or maybe Analog I/O), ultra low power standard data isolators (ADuM1441 or MAX22841), a micro, and 4-20mA DACs in some configuration to suit the application.
Regards,
Jason
At the end yes there will be a redesign, but i found that for the 1B21 i could use the AD693. its not isoltaed but still close to what im looking for.
At the end yes there will be a redesign, but i found that for the 1B21 i could use the AD693. its not isoltaed but still close to what im looking for.