Hi Sir,
1. Can the power-on sequence operate as depicted in the picture below (ADUM2250)?
Power-on sequence: First: Side 2 3.3V (1); Second: Side 1 3.3V (2); Final: Side 1 1.8V (3).

2. Can ADUM2250 operate when I2C1 is pulled high at 1.8 work with VDD1 and VDD2 both are at 3.3V?
It appears that I2C1 is greater than 700mv, then the I2C2 can output high in the picture below. Is it correct?

Thank you~