Post Go back to editing

How to connect CN0401 node to ValueCAN 4-2 or Kvaser Leaf v3 for CAN FD packets sending and receiving?

Thread Summary

The user encountered issues with CAN FD packets being received with CAN ID 0 and zero length when connecting a CN0401 demo setup to ValueCAN 4-2 or Kvaser Leaf v3. The solution involved setting the arbitration bitrate to 500 kbps and data bitrate to 1000 kbps on the external CAN FD devices, and configuring the tx_obj_header_str->ide to 1 for extended CAN ID transmission. However, the user noted that the CN0401 demo code does not explicitly support setting the receive filter for extended CAN IDs, leading to inconsistent reception of short messages.
AI Generated Content
Category: Hardware
Product Number: ADM3055E

We bought two  EVAL-ADM3055EARDZ and two EVAL-ADICUP3029, followed the instructions from

www.analog.com/.../CN0401.pdf

So far have successfully achieved the full CN0401 demo - to have the two CAN nodes talk to each other (as indicated https://www.analog.com/CN0401)

Then we started trying to connect one of this CAN node to ValueCAN 4-2 (or Kvaser Leaf v3), to emulate an engine to produce CAN FD packets, but stopped at first step:

from this CAN node, any messages transmitted through CAN, the far end (ValueCAN or Kvaser) received packets with CAN ID 0 but packets length were always 0.

Would you please suggest or provide any tips/tricks how to set the speed(assumed arbitration 500kbps and data 2Mbps), termination, and any heads up?

Thank you very much.

Mike

Parents
  • Update:

    For whom may be interested, I would like to share my progress:

    1. The other end CAN FD devices, ValueCAN 4-2, or Kvaser Leaf v3, should be set arbitration bitrate to 500k, data bitrate to 1000k, then CN0401 could transceive CAN FD packets up to 64 bytes;

    2. For sending CAN FD packets with extended CAN ID, in the sending function, set the tx tx_obj_header_str->ide to 1, then the other attr eid will be taken as the lower 18 bits of the extended CAN ID, the higher 11 bits come from attr sid. For example: sid = 0x300, eid=0x12345, then the extended CAN ID will be 0xC012345;

    There is still a minor concern while receiving:

    The rx_sid_addr is set to 0x300 in default, but nowhere I can set to enable extended CAN ID for receiving. e.g. how to set it to receive CAN FD packets with a CAN ID 0xC012345?

    Currently both incoming CAN FD packets with 0x300 or 0xC012345 can be received, seems there is no such a setting to specify standard CAN ID or extended CAN ID for receiving. I wonder if that is a feature, or I missed some settings somewhere.

    Thank you very much for your time.

    Mike

Reply
  • Update:

    For whom may be interested, I would like to share my progress:

    1. The other end CAN FD devices, ValueCAN 4-2, or Kvaser Leaf v3, should be set arbitration bitrate to 500k, data bitrate to 1000k, then CN0401 could transceive CAN FD packets up to 64 bytes;

    2. For sending CAN FD packets with extended CAN ID, in the sending function, set the tx tx_obj_header_str->ide to 1, then the other attr eid will be taken as the lower 18 bits of the extended CAN ID, the higher 11 bits come from attr sid. For example: sid = 0x300, eid=0x12345, then the extended CAN ID will be 0xC012345;

    There is still a minor concern while receiving:

    The rx_sid_addr is set to 0x300 in default, but nowhere I can set to enable extended CAN ID for receiving. e.g. how to set it to receive CAN FD packets with a CAN ID 0xC012345?

    Currently both incoming CAN FD packets with 0x300 or 0xC012345 can be received, seems there is no such a setting to specify standard CAN ID or extended CAN ID for receiving. I wonder if that is a feature, or I missed some settings somewhere.

    Thank you very much for your time.

    Mike

Children
  • extra information:

    While connecting to Kvaser Leaf v3, a windows app canecho could echo back CAN FD messages that sent from CN0401 (with extended CAN ID), but noticed that sometimes short message, e.g. "1", "abc", could not reach CN0401 side, but not always. If canecho initiated sending CAN 2.0A messages, then CN0401 received all.

    With two CN0401 connected, then nothing wrong observed.

    Wonder in the CN0401 demo code if the receiving mechanism needs some tricks to set up for receiving all kinds of messages ( CAN FD & CAN messages with or without extended CAN ID)

  • Hello Mike,

       The purpose of the CN0401 is only to demonstrate the ADM3055 in a minimal system and so the CN0401 software is a merely simple driver to the MCP2518 CAN Controller which is what is actually implementing the CAN functionality.   The CN0401 software implements enough functionality to meet this basic goal so that the performance of the ADM3055's PHY layer can be observed.

      You will likely need to consult Microchip's documentation for the MCP2518 and/or other open-source projects which use this part for guidance on how to augment the CN0401 software to utilize the additional functionality the MCP2518 offers.  Searching on the term "MCP2518 driver" will turn up many hits.

    Eric

  • Hello Eric,

    So far the CN0401's verified functionalities are good enough for our purpose.

    We may need dig deeper for a specific project in future.

    Thank you very much.

    Mike

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.