Post Go back to editing

RS-422 compliance

Thread Summary

The user asked if the ADM3064E can be used as an RS422 transceiver. The support engineer confirmed that while RS-485 and RS-422 have similar specifications, the ADM3064E is not suitable for RS-422 due to its receiver input voltage range of -7V to +12V, which does not cover the RS-422 range of -10V to +10V.
AI Generated Content
Category: Datasheet/Specs
Product Number: ADM3064E

Can the ADM3064E be used as the RS422 transceiver?  It is not clear in the documentation.

RS422 support is mentioned on the parts search page

But it is not mentioned on the product's page or in the datasheet