Post Go back to editing

Can ADuM5211 support 1.8V Uart?

Thread Summary

The user inquires if the ADuM5211 supports 1.8V UART, noting the Logic High Input Threshold. The final answer confirms that the ADuM5211 requires VDD1/VDD2 between 3.135V and 5.5V, and suggests considering the ADuM6421A for 1.8V operation.
AI Generated Content
Category: Datasheet/Specs
Product Number: ADuM5211

Hi Sir,

Can ADuM5211 support 1.8V Uart?

In the datasheet, the min of Logic High Input Threshold is 0.7 Viso and 0.7Vdd1. Does this mean chose the lowest for the min value?

For example, Viso is 3.3V and Vdd1 is 5V. Does the min of Logic High Input Threshold is 3.3*0.7=2.31V?

Edit Notes

Add Logic High question.
[edited by: ninasu at 6:39 AM (GMT -5) on 11 Jan 2024]

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.