adm485 not work when power supply connect to 220AC but when disconnect and connect dc socket on board it working
i am using 1 master driver and more than 3 slave receiver by stm32 UC.
ADM485
Production
The ADM485 is a differential line transceiver suitable for high speed bidirectional data communication on multipoint bus transmission lines. It is designed...
Datasheet
ADM485 on Analog.com
adm485 not work when power supply connect to 220AC but when disconnect and connect dc socket on board it working
i am using 1 master driver and more than 3 slave receiver by stm32 UC.
Hi Sabli,
ADM485 is a 5V RS485 transceiver. VCC should be between 5V +/- 5%, 4.75V to 5.25V. The Absolute Maximum Rating for VCC is -0.3V to +7V. Please be sure the supply voltage VCC is within the operating condition. Supply voltage exceeds Absolute Maximum Rating can damage the part.
Best,
Jane
Hello YaoJ
Tanks ToReply
Yes I Know And The VCC Is 5V For ADM485
My Issues is solved By insert Delay in Initial UC peripheral
But Many Time ADM485 Not Working