Post Go back to editing

LTC2871 DC/DC Boost Convertor Control Mechanism

Thread Summary

The user encountered issues with the VDD and VEE rail generation on the LTC2871 transceiver, despite following design guidelines and using recommended components. The final solution was identifying and correcting a schematic error, which resolved the problem of the boost converter switching at almost 100% duty cycle and not generating the correct VDD and VEE voltages.
AI Generated Content
Category: Hardware
Product Number: LTC2871
Software Version: N/A

Hello ADI

A colleague of mine is having issues with the rail generation of the VDD and VEE rails on the LTC2871 transceiver. The design guidelines have been followed for component selection of the capacitors and inductor for the DC/DC convertor. The the Fast Enable (FE) pin is pulled high and the Loop Back (LB) pin is low. Outboard logic drives the state of the RS485/RS232 enable pins (DX232/RX232 & DX485/RX485) and CH2 is pulled high to disable it. Does the part look at anything beyond the state of the RS485/RS232 enable logic when deciding to enable the RS232 rails (VDD & VEE) as it appears to not get enabled as we observe almost 100% duty cycle on the SW pin and 3.3V and 0V on the VDD/VEE pin respectively? 

Sincerely,

Craig MacKinnon

Christie Digital Systems

Kitchener, ON

Canada

   

Thread Notes