My requirement: one image sensor with two display screen.Max9296A portA output to scrren A ,and replicaed portA on portB to the other one screen B.
I have been implemned that max9296 portA output mipi sigal and screen A can display normally.
The problem is that I can not replicated portA on port B successfuly(Port B can not output mipi sigal).
All i did as fellow:
1. enable copy 0 and enable copy 1
2. the source of copy 0 is se to PHY0 and the destination of copy 0 is PHY 2
3.the source of copy 1 is se to PHY1 and the destination of copy 1 is PHY 3
(ohter related seting: 2*4 mode, 4 data lanes for port B )
modify description
[edited by: LangZhong at 11:15 AM (GMT -5) on 21 Nov 2023]