Post Go back to editing

ADM3055E/ADM3057E TX Port Over 1M Data Rate Fail

Thread Summary

The user tested the ADM3055E demo board and observed waveform deformation at data rates above 1 MHz. The final solution was to connect the RS pin to ground for high-speed operation, allowing successful testing up to 12 MHz. The user had initially set the RS pin with a 47K ohm resistor to GND and VIO shorted to VDD1.
AI Generated Content
Category: Hardware
Product Number: ADM3055E/ADM3057E

Hi SIr

I tester EVAL-ADM3055E demo board to fount this chip TX pin data rate over 1MHz the second side output waveform was deformation ,if we need operation at 4MHz or more speed ,ADI have any suggestion?

ADM3055E Second side TX port waveform (Data Rate:1MHz)

ADM3055E Second side TX port  waveform (Data Rate:1.8MHz)

ADM3055E Second side TX port  waveform (Data Rate:3MHz)

Primary side signal generator setting (Vp-p:3.3V Duty:50% ,square wave)

Best

Jack

Edit Notes

Corrected part name typo in title
[edited by: jnaso at 1:03 PM (GMT -5) on 13 Nov 2023]
Parents Reply Children
No Data