ADM3055E
Production
The ADM3055E/ADM3057E are 5kV rms and 3kV rms isolated controller
area network (CAN) physical layer transceivers with integrated
isolated dc-to-dc converters...
Datasheet
ADM3055E on Analog.com
Hi SIr
I tester EVAL-ADM3055E demo board to fount this chip TX pin data rate over 1MHz the second side output waveform was deformation ,if we need operation at 4MHz or more speed ,ADI have any suggestion?
ADM3055E Second side TX port waveform (Data Rate:1MHz)
ADM3055E Second side TX port waveform (Data Rate:1.8MHz)
ADM3055E Second side TX port waveform (Data Rate:3MHz)
Primary side signal generator setting (Vp-p:3.3V Duty:50% ,square wave)
Best
Jack
Hi Jack,
What is the state of the RS pin? JP4 on the EVAL-ADM3055EEBZ will set the part in and out of slope control mode.
Regards,
Jason
Hi Jnaso,
This test case RS pin is 47K ohm resistor to GND ,and VIO short to VDD1 ,SILENT STBY AUXIN pins to Low.
Best
Jack
Hi Jack,
Connect the ADM3055E's RS pin to ground for high speed data. This is likely the reason for the distorted waveform on the CAN bus. Please refer to the ADM3055E datasheet Pin Configuration section. There is also a subsection about the RS pin in Theory of Operation which will describe the operation in greater detail.
Slope control mode should only be used for low data rates.
Regards,
Jason
Hi Jnaso.
Thanks for your support ,I can TX port test to 12MHz.
Best
Jack