LTC6820
Production
The LTC6820 provides bidirectional SPI communications between two isolated devices through a single twisted-pair connection. Each LTC6820 encodes logic...
Datasheet
LTC6820 on Analog.com
Hi, I am using LTC6820 to isolate the interface between STM32F446re microcontroller to LTC6811. The connections for LTC6820 is as follows
MSTR = VDD,
EN = VDD,
SLOW = GND,
POL, PHA = VDD.
All the remaining connections are according to the datasheet specifications mentioned. But I am unable to transmit or receive signals on IP or IM pins.
Can you guide me how to start communication.
Moved from How to Use EngineerZone to Interface and Isolation on Wednesday, November 8, 2023 3:33:08 PM by emassa