Post Go back to editing

MAX9947 high temperature

Thread Summary

The user inquires about the MAX9947 failing to operate in a 70°C environment when used to replace the SN65HVD62 without changing the peripheral circuits. The final answer indicates that only Maxim ATE products are currently supported on EngineerZone, and directs the user to visit the technical support pages for further assistance with Maxim Integrated products.
AI Generated Content
Category: Hardware
Product Number: MAX9947

Dears

   My customer use MAX9947 to replace SN65HVD62, Customer don't change the peripheral circuits.

When customer put the MAX9947 board into the 70℃  environment, it can't work.  But competitor SN65HVD62 can operate well. 

Can you check it and give some advise ? 

Edit Notes

tagged
[edited by: GenevaCooper at 9:46 PM (GMT -5) on 1 Dec 2023]
Parents Reply Children
No Data