KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
MAX9947
Production
The MAX9947 is an AISG-compliant, fully integrated transceiver.
The MAX9947 receiver offers a typical dynamic range of 20dB and integrates a bandpass...
Datasheet
MAX9947 on Analog.com
Dears
My customer use MAX9947 to replace SN65HVD62, Customer don't change the peripheral circuits.
When customer put the MAX9947 board into the 70℃ environment, it can't work. But competitor SN65HVD62 can operate well.
Can you check it and give some advise ?

Hi, Thank you for your inquiry. Only Maxim ATE products are supported on EngineerZone at this time. Over the next several months, you will see more Maxim products being supported in EngineerZone. Please visit one of the technical support pages on our newly integrated website below for assistance with Maxim Integrated products.
EN - https://www.analog.com/en/support/technical-support.html#
CN - https://support.analog.com/zh-CN/technical-support/
JP - https://support.analog.com/ja-JP/technical-support/