Category: Hardware
Product Number: ADUM4195
Software Version: LTSpice
Hello,
- I just wanted to confirm, can the ADUM4195 be used to provide control loop isolation (isolating primary & secondary GNDs) in PSU applications?
- Can you confirm that the minimum and maximum beginning of life unity gain variation is -0.5%/+0.5% for 1V/V?
- I'm not familiar with the different nomenclature used for the device. Does ADI have or plan on introducing an "enhanced plastic (EP)" or rad-hard version of this amplifier?
- The LTSpice model for the ADUM4195 differs from the schematic symbol shown on the datasheet...
The datasheet only describes and depicts VIN, VOUT, VDD1, VDD2, SHTD... What is the difference between "VOUT1" and "VOUT2" on the LTSpice version? What does "REF1" and "REF2" entail?
Thanks