Post Go back to editing

ADUM130E1BRWZ is dropping pulses

Category: Hardware
Product Number: ADUM130E1BRWZ

Hello,
I have a problem with the ADUM130E1BRWZ. I am designing a half-bridge circuit and using this circuit to isolate my signals. The signals are generated from a microcontroller, it is a PWM signal, frequency 100 kHz. The output of the ADUM130E1BRWZ is connected directly to the half-bridge driver. The signal on the input to ADUM130E1BRWZ is ok, but the ADUM130E1BRWZ keeps dropping some pulses. This happens only on one of the channels (channel HIN in the schematic). I have checked the voltage with an oscilloscope on the enable and VCC, both are straight DC voltages, no voltage drops there. Attached is a partial schematic, PCB and oscilloscope measurement (Ch1 is input, Ch2 is output from the ADUM. The problem appears even when the half-bridge is not powered, even when the half-bridge driver is unsoldered from the PCB and hence the ADUM130E1BRWZ is not loaded with anything. So I think it can´t be interference from the half-bridge. The problem does not appear all the time, but when it happens it happens with a frequency of about 7.5 kHz. The used oscilloscope has all channels galvanically isolated.
Please any ideas what could be the cause and how to solve the problem ?