Post Go back to editing

Hot-plug CAN application with ADM3058E transceiver

Thread Summary

The user asked if the ADM3058E supports hot-plug applications. The final answer confirms that the ADM3058E is compatible with hot-plug due to its bus pins being in high-Z state when VDD2 is off, and in the recessive state until VDD1 is present and TxD is asserted low.
AI Generated Content
Category: Datasheet/Specs
Product Number: ADM3058E

Hi, 

I need to select the right CAN transceiver for an application and the question is: did ADM3058E support hot-plug application ? 

Thanks

Luci

  • Hello Luci,

       Yes, the ADM3058E should be compatible with hot-plug applications since its bus pins are high-Z when the VDD2 supply is off.  When the VDD2 supply is present, the bus pins will be in the recessive state until both VDD1 is present and TxD is asserted low.  Connecting the ADM3058 to an active bus when in either the high-Z or recessive states should not disturb the bus.

    Eric