Hi team,
Customer wants to verify if this device output can protect against short to VCC(32V) or Ground? (2A max)
Also, if it's comply with TIA-232-F?
If not, any other RS232 device can do so?
Thx a lot!!
Regards,
Andrew
MAX13223E
Production
The MAX13223E is a +3.0V to +5.5V-powered EIA/TIA-232 and V.28 communications interface with fault protection on the RS-232 line interface. This allows...
Datasheet
MAX13223E on Analog.com
Hi team,
Customer wants to verify if this device output can protect against short to VCC(32V) or Ground? (2A max)
Also, if it's comply with TIA-232-F?
If not, any other RS232 device can do so?
Thx a lot!!
Regards,
Andrew
Hi Andrew,
MAX13223E has +/-70V overvoltage protection on R1IN, R2IN, T1OUT, and T2OUT pins, however the output short-circuits current is limited to +/-80mA.
The part is complied with TIA-232-F issued in 1997.
Regards,
Hi Andrew,
MAX13223E has +/-70V overvoltage protection on R1IN, R2IN, T1OUT, and T2OUT pins, however the output short-circuits current is limited to +/-80mA.
The part is complied with TIA-232-F issued in 1997.
Regards,