Post Go back to editing

Could you please provide guidance on how to utilize separate GNDs with MAX14919?

Thread Summary

The user wants to separate PGND and GND for the MAX14919, but the datasheet specifies that both must be connected to the EP pin. The recommended solution is to connect PGND/GND to system COM via an external NMOS to protect against reverse current, as shown in the datasheet on page 17.
AI Generated Content
Category: Hardware
Product Number: MAX14919

I want to separate a PGND and GND.

From the datasheet, The EP pin has to connect with PGND and GND.
I want to separate PGND and GND.

Can I use it like the attached picture?

  • Hi,

    The GND and PGND pins should be connected to EP for MAX14919 to operate normally. They cannot be separated. 

    If a COM ground is required in the system, we recommend connecting the PGND/GND of the MAX14919 to system COM via an external NMOS, so the system can be protected from reverse current. Refer to the diagram in datasheet page 17. Is this the reason that we need separate grounds?

    Thanks,

    Wei

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.