Post Go back to editing

ADUM4121. PWM connection. Can a LVDS be connect directly to Vi+ and Vi- (by using the twisted pair) without a receiver?

Category: Hardware
Product Number: ADUM4121

I'm using an ADUM4121 as a gate driver for a SiC MOSFET device.

I have seen two examples of how to use the VI+ and VI- pins for the PWM.

1.- Connecting the VI- pin to the ground and applying the logic to the VI+.

2.- Not connecting VI- to the ground and to applying complementary pulses to VI+ and VI-.

I was exploring a third option.

3.- Does the pin VI+ and VI- work as a differential input? I was thinking of using a differential line voltage driver connected to the PWM source in order to use longer twisted pair cables and the other end (twisted pair to VI+ and VI- respectively), and wondering if I could connect this twisted pair directly to VI+ (one cable) and to VI-(the other cable) as if working as a differential input.

This alternative could help me to save a receiver for the line voltage differential driver.

Is it possible to make this type of connection? Do the VI+ and VI- work as differential input? 

Thank you!

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.