KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
ADuM4121
Production
The ADuM4121/ADuM4121-1 are 2 A isolated, single-channel drivers that employ Analog Devices, Inc.’s iCoupler® technology to provide precision isolation...
Datasheet
ADuM4121 on Analog.com
ADM4168E
Production
The ADM4168E is a dual RS-422 transceiver suitable for high speed communication on point to point and multidrop transmission lines. The ADM4168E is designed...
Datasheet
ADM4168E on Analog.com
I'm using an ADUM4121 as a gate driver for a SiC MOSFET device.
I have seen two examples of how to use the VI+ and VI- pins for the PWM.
1.- Connecting the VI- pin to the ground and applying the logic to the VI+.
2.- Not connecting VI- to the ground and to applying complementary pulses to VI+ and VI-.
I was exploring a third option.
3.- Does the pin VI+ and VI- work as a differential input? I was thinking of using a differential line voltage driver connected to the PWM source in order to use longer twisted pair cables and the other end (twisted pair to VI+ and VI- respectively), and wondering if I could connect this twisted pair directly to VI+ (one cable) and to VI-(the other cable) as if working as a differential input.
This alternative could help me to save a receiver for the line voltage differential driver.
Is it possible to make this type of connection? Do the VI+ and VI- work as differential input?
Thank you!
Hi PabloGuicharrousse,
Both the VI+ and VI− pins use CMOS logic level inputs and are not meant to be compatible with differential signals.
You wont get the benefit of common mode rejection as by using a balanced transmission lines.
I recommend to consider ADM4168E for a robust differential communication.
Regards,
Thanks for your help!