Post Go back to editing

Controller Area Network (CAN) transceiver

Thread Summary

The user inquired about the compliance of the MAX3058/3059 CAN transceiver with ISO 11898-1, 11898-2, or ARINC 825 standards. The final answer suggested using ADI's latest CAN transceivers, such as LTC2875, MAX13053A, or MAX33054E, for new aerospace applications. No specific compliance information was provided for the MAX3058/3059.
AI Generated Content
Category: Software
Product Number: MAXIM CAN Transceiver MAX3058/3059

Hi,

I'm looking to use MAXIM CAN Transceiver MAX3058/3059 in an aerospace application which requires that it is compliant with standards

ISO 11898-1 and 11898-2, or with standard ARINC 825. The data sheet does not mention standards. Does the part meet any of those standards?                  Thanks

Edit Notes

Moved and updated tags
[edited by: Sara Campbell at 3:59 PM (GMT -4) on 5 Jul 2023]
Parents Reply Children
No Data