Hello
What is the max output current of the MAX6817EUT+T?
Thank you
Gary
KCC's Quizzes AQQ306 about a fish stick challenge
1. First the quote of the month: " I am so clever that sometimes I don't understand a single word of what I am saying" - Oscar Wilde
2. New quiz AQQ306 about a fish stick challenge:
Here below is a pseudo fish diagram swimming to the right.
Question
View All
October Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Finding Your Circuit Chi — EMC Quiz!
Think you know EMC? Test your knowledge with our 5-question quiz!
Read the blog first, then take the challenge: Finding Your Circuit Chi
Every current flowing creates electromagnetic fields.
Strong EMC design
View All
MAX6817
Production
The MAX6816/MAX6817/MAX6818 are single, dual, and octal switch debouncers that provide clean interfacing of mechanical switches to digital systems. They...
Datasheet
MAX6817 on Analog.com
Hello
What is the max output current of the MAX6817EUT+T?
Thank you
Gary
MAX6817 datasheet Electrical Characteristics table gives test conditions for OUT logic levels VOL, VOH. For logic high output, VOH will be within 1.0V of VCC, for loads that require MAX6817 to source up to 0.4mA; and for logic low output, VOL will be less than 0.4V for loads that require MAX6817 to sink up to 1.6mA. The output impedance is non-linear because it's a digital output.
So MAX6817 can directly sink 1.6mA, and it can also source up to 0.4mA.