Post Go back to editing

Relationship between MAX14917 VDD and OUT_x output voltage

Thread Summary

The user inquired about driving the OUT_x pin of the MAX14917 with VDD at 15V. The final answer confirmed that the MAX14917 operates normally with VDD=15V, as long as it does not drop below the VDD UVLO Fall threshold of 8V. The VDD UVLO Rise threshold is 9.6V, and the device will function as expected if VDD remains above 10V after power-up.
AI Generated Content
Category: Hardware
Product Number: MAX14917

I'm considering the MAX14917.
So I have one question.

Is it possible to drive the OUT_x pin if the VDD pin is driven with 15V?

I'm considering using it with VDD = 15V.
In Power Up and Undervoltage Lockout on page 12 of the datasheet,
It looks like you wrote that when VDD_GOOD_R exceeds 16V, /VDDOK goes low, outputting the OUT_x pin.
/VDDOK pin is not used.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.