Post Go back to editing

Relationship between MAX14917 VDD and OUT_x output voltage

Thread Summary

The user inquired about driving the OUT_x pin of the MAX14917 with VDD at 15V. The final answer confirmed that the MAX14917 operates normally with VDD=15V, as long as it does not drop below the VDD UVLO Fall threshold of 8V. The VDD UVLO Rise threshold is 9.6V, and the device will function as expected if VDD remains above 10V after power-up.
AI Generated Content
Category: Hardware
Product Number: MAX14917

I'm considering the MAX14917.
So I have one question.

Is it possible to drive the OUT_x pin if the VDD pin is driven with 15V?

I'm considering using it with VDD = 15V.
In Power Up and Undervoltage Lockout on page 12 of the datasheet,
It looks like you wrote that when VDD_GOOD_R exceeds 16V, /VDDOK goes low, outputting the OUT_x pin.
/VDDOK pin is not used.

Parents
  • Yes, the MAX14917 works normally with VDD=15V. Regardless of /VDDOK indicator is used or not, the internal logic monitors the VDD level and compares it with the VDD UVLO threshold. As shown in Figure 3 on page 12, as soon as VDD falls below the VDD UVLO threshold, the OUTs will be shut down (off). In this case, you will need to raise VDD above 16V to resume the OUT operation. However, if you don't reach UVLO threshold after power up, the MAX14917 operates normally as soon as the VDD is above 10V. 
    It is recommended to monitor /VDDOK signal to prevent automatic shutdown of OUT_ in case of heavy load that can drop the VDD below the UVLO threshold.

  • Thank you for your answer. I mostly understood.
    I have an additional question.

    >However, if you don't reach UVLO threshold after power up,
    the MAX14917 operates normally as soon as the VDD is above 10V.

    Does this mean when the VDD UVLO Fall Threshold is above 7.9V and below 9.6V after power up?

    When you say VDD exceeds 10V, are you referring to the VDD UVLO Rise Threshold of 9.6V?

    Best regards,

    Yuya

  • Yes, your understanding is correct. The VDD UVLO Fall threshold is about 8V (7.9V min). When VDD falls below VDD UVLO Fall threshold, the OUTs will be turned OFF. However, the VDD UVLO Rise threshold is 9.6V max. After this point the MAX14917 starts to operate normally if no VDD UVLO Fall events. That is why the VDD Supply Voltage (normal operation spec) is from 10V to 36V.

    Best Regards,

    Yuriy

Reply
  • Yes, your understanding is correct. The VDD UVLO Fall threshold is about 8V (7.9V min). When VDD falls below VDD UVLO Fall threshold, the OUTs will be turned OFF. However, the VDD UVLO Rise threshold is 9.6V max. After this point the MAX14917 starts to operate normally if no VDD UVLO Fall events. That is why the VDD Supply Voltage (normal operation spec) is from 10V to 36V.

    Best Regards,

    Yuriy

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.