Post Go back to editing

Question about ADM2486 fail-safe

Category: Hardware
Product Number: ADM2486

Hello,

I have some questions about the fail-safe function of the ADM2486.

How is the fail-safe realized in spite of the specification of ±200mV differential input threshold voltage?

Also, is it necessary to add any external circuit for fail-safe when the A and B inputs are shorted?

Best Regards,

Kazu

Parents
  • The ADM2486s fail-safe feature works by providing a small bias to the A & B pins which will keep Va-Vb >200mV when the A & B pins are open circuited.

    If the A & B pins are shorted together, then the receiver input voltage will presumably be within the +/-200mV and the output will be indeterminant.

    If you need fail-safe operation under a shorted bus condition, then I'd suggest using one of our other parts with an asymmetric threshold voltage, such as the MAX14938/9

    Eric

Reply
  • The ADM2486s fail-safe feature works by providing a small bias to the A & B pins which will keep Va-Vb >200mV when the A & B pins are open circuited.

    If the A & B pins are shorted together, then the receiver input voltage will presumably be within the +/-200mV and the output will be indeterminant.

    If you need fail-safe operation under a shorted bus condition, then I'd suggest using one of our other parts with an asymmetric threshold voltage, such as the MAX14938/9

    Eric

Children
No Data