Post Go back to editing

Input hysteresis of ADuM14X and ADuM24X

Category: Datasheet/Specs
Product Number: ADuM240

When I look at the block diagram such as the datasheet figure 1, it seems that the input has a hysteresis characteristic.

Does the input voltage have hysteresis characteristics?
If yes, what is the voltage

Parents
  • Hi Uboti, 

    There is hysteresis built into the input of the ADuM24xE and it scales based on the supply voltage. Input hysteresis will typically be around 0.4V for a 1.8V supply, 0.6V for 2.5V, 0.8V for 3.3V, and 1.5V for 5V supply. 

    FYI, the new pin-compatible ADuM340E isolators have an input hysteresis specification provided in the datasheet. 

    Regards,

    Jason 

Reply
  • Hi Uboti, 

    There is hysteresis built into the input of the ADuM24xE and it scales based on the supply voltage. Input hysteresis will typically be around 0.4V for a 1.8V supply, 0.6V for 2.5V, 0.8V for 3.3V, and 1.5V for 5V supply. 

    FYI, the new pin-compatible ADuM340E isolators have an input hysteresis specification provided in the datasheet. 

    Regards,

    Jason 

Children