Post Go back to editing

Output Power of LTM2884CY#PBF

Category: Hardware
Product Number: LTM2884CY#PBF

Hi,

We are using LTM2884CY#PBF for USB isolation in one of our product. Input supply of LTM2884CY#PBF IC is 5V. As per datasheet, output would be 5V, 200mA for stated input voltage. Our requirement is 500mA max. So we are using an extra DC-DC power isolator to take more power. Can anyone suggest the better solution for that? We want to use only one module for USB isolation with 5V, 500mA output at 5V input supply. 

Thanks.



tag
[edited by: lallison at 6:56 PM (GMT -4) on 8 May 2023]