I am using the ADUM141E1 part in a design. The VDD1 supply voltage is 5 volts. The VDD2 supply voltage is 3.3 volts.
I don't understand the quiescent current entries, pasted below. This is from page 3 of the Rev D datasheet for this part. Why are there four rows?
I mean, the conditions in the rightmost column for the first two rows are identical (Vi = 0 (E0, D0), 1 (E1, D1). Are there more conditions that are not listed in these rows?
What is the max ADUM141E1 quiescent current with Vi =0? Is it 17.0 mA or 10.0 mA?