Hi,
I use VISO as a power supply for OUT signals pull-up as shown below.
Is it OK to connect two ADuM6400 VISOs together?
Regards,
Kazu
ADUM6400
Production
The ADuM640x devices are quad-channel digital isolators with isoPower®, an integrated, isolated DC/DC converter. Based on the Analog Devices, Inc., iCoupler...
Datasheet
ADUM6400 on Analog.com
Hi,
I use VISO as a power supply for OUT signals pull-up as shown below.
Is it OK to connect two ADuM6400 VISOs together?
Regards,
Kazu
Hi Kazu,
There is no issue connecting VISOs together, however the device with the higher output voltage will provide all (most) of the load current. In other words, the two parts will not share the load current equally, as the load demand increases the parts will tend to share more equally.
There are other parts in the is product family which do support load sharing, such as the ADuM5401 which has an RCout pin which can be connected to the RCin pin of an ADuM5202. Depending on the voltage isolation required, I can assist in finding parts that can help with your schematic.
Regards,
Amit
Hi Kazu,
There is no issue connecting VISOs together, however the device with the higher output voltage will provide all (most) of the load current. In other words, the two parts will not share the load current equally, as the load demand increases the parts will tend to share more equally.
There are other parts in the is product family which do support load sharing, such as the ADuM5401 which has an RCout pin which can be connected to the RCin pin of an ADuM5202. Depending on the voltage isolation required, I can assist in finding parts that can help with your schematic.
Regards,
Amit