Post Go back to editing

MAX31915 input logic levels; supply recommendations

Category: Hardware
Product Number: MAX31915

Datasheet does not describe logic levels for DB0 and DB1 logic inputs. Is it CMOS or TTL level? Next, supply level for Vcc24V pin is up to 45V (max 36V recommended), but typical application circuit shows additional required serial 150 Ohm resistor. What is function of this resistor?

Parents
  • Hi,

    DB0 and DB1 are 5V CMOS logic inputs, referenced to GND and roughly centered at 2.5V.

    150ohm resistor is a current limiting resistor protecting the VCC24V from overcurrent condition, for example lightning surge transients. The VCC24V supply current is small, 2.3mA max when 5VOUT is not loaded, so the 150ohm won't create too much voltage drop on the supply line.

    if large 5VOUT load current is required in the application, we can replace D0 with a TVS diode and remove the 150ohm from the circuit. During high voltage transients, the TVS diode will clamp the voltage to a safe level while conducting to absorb the excessive current.

    Thanks,

    Wei

  • Thank you. Final question - is it possible to drive DB0 and DB1 from 3.3V logic (STM ARM processor)?

  • I took a look at the logic input specs of another digital input chip, MAX31913, that share the same DB0/DB1 and 5VDOUT design.

    Here is the VIH/VIL spec. BTW this is not a conventional way to spec VIH and VIL...

    The input high spec is 0.7*V5VOUT = 0.7*5.25 = 3.675V max. We couldn't guarantee the 3.3V logic would work over the process variation and operating temperature ranges.

    Thanks,

    Wei

Reply
  • I took a look at the logic input specs of another digital input chip, MAX31913, that share the same DB0/DB1 and 5VDOUT design.

    Here is the VIH/VIL spec. BTW this is not a conventional way to spec VIH and VIL...

    The input high spec is 0.7*V5VOUT = 0.7*5.25 = 3.675V max. We couldn't guarantee the 3.3V logic would work over the process variation and operating temperature ranges.

    Thanks,

    Wei

Children