Post Go back to editing

RS485 IC (MAX22028FAWA)

Category: Hardware
Product Number: MAX22028FAWA

Hi,

The data will be transmitted over the RS485 IC (MAX22028FAWATx ) TX pin, then it will loop back over the IC's RX pin.

How to solve the issue?

Regard,

Vijay

Edit Notes

added tag LMXMprodsupport
[edited by: GenevaCooper at 2:46 PM (GMT -5) on 23 Feb 2023]
Parents Reply
  • I believe you are using the wrong chip, the 22028 is meant to have the Rx pin follow the Tx pin, if you still want the high speed version but not have the Rx pin follow the differential line then use the MAX22026.  Page 22 of the Rev 8 data sheet has a table that indicates which chips have Rx follow VA-VB when the driver is active.

Children
No Data