Hello,
I am looking at the MAX77751 to manage charge of 2 Lithium cell in parallel (1S2P).
Batteries are 2450mA each so a total of 6800mAh.
Each recharge with a current of 1.475A
Some questions:
Can I place simply these 2 cells in parallel and use the MAX77751 ?
Do I need additional feature protection (temperature cell ?) ?
Any balancing to add ?
How can I ensure cells will be charged before 6 hours limits set by the MAX77751 ?
Many thanks in advance
Phil
Edit Notes
Added Tag: LMXMprodsupport[edited by: GenevaCooper at 6:44 PM (GMT -5) on 20 Jan 2023]