Hello,
This component LTC2877HDD#PBF vorks with 3V to 5 V, does it have same performances at receive and transmit data at 3V and 5V ? (transmission signal strength ?)
Regards,
Bruno.
KCC Quizzes AQQ303 about the radius of a circle
1. Quote of the month: "When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his car" - Will Rogers
2. Quiz AQQ304 about finding the radius of a circle
Good luck, and try to be
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
LTC2877
Production
The LTC2876 and LTC2877 are PROFIBUS RS485 transceivers designed to meet the test specifications for PROFIBUS-DP masters and PROFIBUS-DP slaves, fully...
Datasheet
LTC2877 on Analog.com
Hello,
This component LTC2877HDD#PBF vorks with 3V to 5 V, does it have same performances at receive and transmit data at 3V and 5V ? (transmission signal strength ?)
Regards,
Bruno.
Hi Bruno,
There are certain specifications in the EC table that will vary given the supply voltage. If there are such dependencies, the Conditions column will have more clarity. For example, the differential output driver voltage will depend on the VCC supply and this is shown below:

If there is no differentiation specified in the Condtiions column, then they should be valid for both VCC = +3.3V or +5V.
Regards,
Omar
Hello Omar,
Thanks very much for your answer.
Regards,
Bruno.