Post Go back to editing

ADN4624 HDMI reference design

Thread Summary

The user inquired about capacitor and resistor values for an HDMI isolation circuit using ADN4624. The support engineer provided a similar circuit note (CN0422) using ADN4654 and suggested optimizations, including using AC coupling capacitors only on the outputs and simplifying LVDS common mode biasing with 50 Ohm resistors to 1.8V VDD1. The user then shared a schematic for review, which was not explicitly confirmed as correct.
AI Generated Content
Category: Choose a category
Product Number: ADN4624

Hi ADI team

In ADN4624 datasheet Page 19,show the HDMI example diagram

I'd like to know the capacitor and resistor value,is the detail schematic document?

Thanks

  • Hi Larson,

    We have not yet published a complete tested solution using ADN4624 to isolate HDMI, but I can refer you to our circuit note using ADN4654:

    CN0422 Circuit Note | Analog Devices

    Using ADN4624 will be similar but allowing higher bandwidth so that 1080p resolution is practical (or maybe half-frame rate 4K).

    Some suggested optimizations of that circuit would be to only use the AC coupling capacitors on the outputs (don't place the 10k pull-up/pull-down resistors), and on the inputs, the pull-ups can be to the 1.8V VDD1 supply. The LVDS common mode biasing can be simplified, by omitting the 10k pull-up/pull-downs and instead splitting the termination resistor (connecting between two resistors to 1.8V). With this arrangement, it should be sufficient to terminate simply with 50 Ohm to 1.8V on Din+ and on Din-, after the AC coupling cap (with no pull-up before it).

    Best regards,

    Conal

  • Hi Conal

    Based to your suggestion,attached schematic is right?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.