Post Go back to editing

Using Can FD with Standard CAN 2.0AB traceivers

Category: Datasheet/Specs
Product Number: ADM3051
Software Version: na

Hi ,

I just want to make sure about using  CAN-FD on a CAN2.0 Tranceiver like ADM3051, in essense CAN-FD is high speed with Flexible data rate .

However if you still run CAN-FD at 1Mbit can you still use a CAN2.0AB traceiver? also the reverse question, can you use a CAN2.0AB  with CAN-FD tranceiver?

regards

Conrad

Parents
  • Hi Conrad, 

    A CAN-FD transceiver can be used in a CAN2.0B or CAN2.0A network. CAN-FD compliant transceivers will be backwards compatible. The reverse may not necessarily be true. For a CAN FD network, I recommend evaluating the LTC2875 which is available in an 8L-SOIC_N pin-compatible with the ADM3051.  

    Regards,

    Jason

Reply
  • Hi Conrad, 

    A CAN-FD transceiver can be used in a CAN2.0B or CAN2.0A network. CAN-FD compliant transceivers will be backwards compatible. The reverse may not necessarily be true. For a CAN FD network, I recommend evaluating the LTC2875 which is available in an 8L-SOIC_N pin-compatible with the ADM3051.  

    Regards,

    Jason

Children
No Data