Post Go back to editing

ADP1031 maximum output current

Category: Hardware
Product Number: ADP1031

Hello,

I'm planning to use the ADP1031 for realizing an isolated analog output. However I have difficulties to reach the needed output current IVOUT1(MAX) of 30mA

I want to use following values:

VINP=6V or 24V

VOUT1=15V

VOUT2=5V

VOUT3=-15V

LPRI=280µH

Using above values and interim results from other formulas in the datasheet, I calculate following values with the formula on page 32:

IVOUT1(MAX)=14,1mA for VINP=6V and 20,1mA for VINP=24V

Both are considerably below the needed 30mA. Can you help me to increase IVOUT1(MAX) or is the part not suited for such a output current?