Hello,
I'm planning to use the ADP1031 for realizing an isolated analog output. However I have difficulties to reach the needed output current IVOUT1(MAX) of 30mA
I want to use following values:
VINP=6V or 24V
VOUT1=15V
VOUT2=5V
VOUT3=-15V
LPRI=280µH
Using above values and interim results from other formulas in the datasheet, I calculate following values with the formula on page 32:
IVOUT1(MAX)=14,1mA for VINP=6V and 20,1mA for VINP=24V
Both are considerably below the needed 30mA. Can you help me to increase IVOUT1(MAX) or is the part not suited for such a output current?