Is the following protection circuit suitable for ADM3251E?

KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
ADM3251E
Production
The ADM3251E is a high speed, 2.5 kV fully isolated, single-
channel RS-232/V.28 transceiver device that operates from a
single 5 V power supply. Due to...
Datasheet
ADM3251E on Analog.com
Is the following protection circuit suitable for ADM3251E?

Hi Lijie,
Topologically, this protection circuit will protect against surges up to the limits of the gas discharge tube; however, the particular TVS diode selection is inappropriate for the ADM3251E.
The SMBJ26CA's trigger voltage is approximately 32V @1mA and its maximum clamping voltage is 42V@14A. The TBU will limit the transient current to its trigger current of approximately 200mA, so the SMBJ26CA's working clamp voltage will be someplace between 32 and 42V.
The ADM3251E's receiver's R_IN ABSMAX is +/-30V and transmitter's T_OUT ABSMAX is +/-15V and so the transient voltage the SMBJ26CA will allow will exceed the ABSMAX for the ADM3251E likely resulting in damage.
To properly protect the ADM3251E's receiver, I'd suggest using the SMBJ18CA which has a reverse standoff voltage of 18V (greater than the RS-232 spec of 15V) and a max clamping voltage of 29.2V which is less than the 30V ABSMAX.
For the transmitter, the normal output swing is +/-5.7V and the typical output short-circuit current is 12mA (which is less than the RS-232 specification that it is to be less than or equal to 100mA). Since the TBU's trigger current is ~200mA, it will not trigger when there is a line short and will only trigger when there is an external surge. Since the transmitter is supposed to be the only generator on this circuit, we can choose a TVS based on its ratings and there are many different options. I'd suggest the SMBJ8.5CA which has a reverse standoff of 8.5V and a max clamping voltage of 14.4V.
Eric
Hi Lijie,
Topologically, this protection circuit will protect against surges up to the limits of the gas discharge tube; however, the particular TVS diode selection is inappropriate for the ADM3251E.
The SMBJ26CA's trigger voltage is approximately 32V @1mA and its maximum clamping voltage is 42V@14A. The TBU will limit the transient current to its trigger current of approximately 200mA, so the SMBJ26CA's working clamp voltage will be someplace between 32 and 42V.
The ADM3251E's receiver's R_IN ABSMAX is +/-30V and transmitter's T_OUT ABSMAX is +/-15V and so the transient voltage the SMBJ26CA will allow will exceed the ABSMAX for the ADM3251E likely resulting in damage.
To properly protect the ADM3251E's receiver, I'd suggest using the SMBJ18CA which has a reverse standoff voltage of 18V (greater than the RS-232 spec of 15V) and a max clamping voltage of 29.2V which is less than the 30V ABSMAX.
For the transmitter, the normal output swing is +/-5.7V and the typical output short-circuit current is 12mA (which is less than the RS-232 specification that it is to be less than or equal to 100mA). Since the TBU's trigger current is ~200mA, it will not trigger when there is a line short and will only trigger when there is an external surge. Since the transmitter is supposed to be the only generator on this circuit, we can choose a TVS based on its ratings and there are many different options. I'd suggest the SMBJ8.5CA which has a reverse standoff of 8.5V and a max clamping voltage of 14.4V.
Eric