Post Go back to editing

What is the maximum cable length for part ADN4655

Category: Hardware
Product Number: ADN4655
Software Version: NA

I am using ADN4655 part to isolate SerDes lines (1GHz) coming from FPGA and output to a cable to be later connected to another component. I wanted to know what is the maximum cable length this part can drive assuming the cable is shielded and uses twisted pair as well as it has impedance matching of ~100ohms.

How does the frequency affect the maximum cable length as well?

This also assumes all the termination resistors are placed near the Rx.

The following is illustrated in this block diagram:

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.