I am using ADN4655 part to isolate SerDes lines (1GHz) coming from FPGA and output to a cable to be later connected to another component. I wanted to know what is the maximum cable length this part can drive assuming the cable is shielded and uses twisted pair as well as it has impedance matching of ~100ohms.
How does the frequency affect the maximum cable length as well?
This also assumes all the termination resistors are placed near the Rx.
The following is illustrated in this block diagram: