Post Go back to editing

ADM3053 CAN Response Issue

Thread Summary

The user encountered issues with the ADM3053 transceiver where the return signal appeared as garbage pulses at 500kbps. The problem was resolved by reducing the size of EMI filter capacitors at the connector, which were too large for the high-speed CAN signal. An accompanying suggestion noted that the 47k Rs resistor could also affect the driver slew rate and recommended reducing it for faster edge rates.
AI Generated Content
Category: Hardware
Product Number: ADM3053
Software Version: N/A

Hello, I am encountering an interesting issue when testing my circuit board, which uses the ADM3053 transceiver. The signal being sent to the transceiver (scoped on the isolated GND2 side) appears to be very nice, but the acknowledgement and return signal sent by the ADM3053 appears to be garbage (strange pulses that don't even look like CAN data). Right now it seems like the root cause lies somewhere in the hardware configuration, but I can't seem to figure out anything I did that's outside the recommendations of the datasheet. The speed of the communication is set up to be 500kbps. I have attached images below of my CAN schematic and the oscilloscope CAN waveforms. If anyone has seen something like this before and might have an idea of what could cause weird behavior like this, your expertise is greatly appreciated.